VBUS.THREEPHASE

Description

This parameter indicates whether the AC line input is single or three phase, and whether phase loss detection is active.


  • Setting this parameter to 1/0 can enable/disable “phase loss” detection but it will not disable “power loss” detection.

“Power loss” condition is the condition where there is a sudden drop in the AC mains voltage. If this condition occurs, Fault 2014: AC input phase loss gets detected, inrush relay is opened, and the user must wait until VBUS.VALUE drops below VBUS.INRUSHOFF to clear the fault.

This mechanism is designed to protect the drive and fuse against potential damages due to sudden drops in the AC mains voltage.

Examples

Usage

If the parameter is set to 0, the drive assumes that the AC line input is single phase, and phase loss detection is turned off.

If the parameter is set to 1, the drive assumes that the AC line input is three phase, and phase loss detection is turned on. If the drive detects a phase loss condition and an axis is enabled, it throws Fault 2014: AC input phase loss on each axis.

Code

--> VBUS.THREEPHASE 1
--> DRV.FAULTS
1-2014: AC input phase loss.
2-2014: AC input phase loss.


--> VBUS.THREEPHASE 0
--> DRV.FAULTS
No faults active

Context

For more information on DC bus protection, refer to Power View and Regeneration.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 (single phase) to 1 (three phase)
Default Value 1 (three phase)
Data Type Integer
See Also VBUS.VALUE
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
VBUS.THREEPHASE

300ah

09h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

VBUS.THREEPHASE

2509

9CD

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.THREEPHASE

2509

Unsigned8

Read/Write

-